|
Secure,
Reliable, Practical - A solid connection with Bulgin
Farnell InOne and Bulgin
Farnell InOne are pleased to introduce the New Polysnap,
Power Inlet Modules and Buccaneer Sealed Lan-Ethernet Connectors
from Bulgin. Bulgin Components are one of Farnell InOne's
longest standing and valued suppliers with a justified
reputation for the design and manufacture of high quality
products.
Polysnap mains
interface modules with circuit breakers
A
range of re-settable mains inlet modules. EN60320 type
connectors have become a standard mains interface for many
products from white and brown goods through to industrial,
medical and business equipment. This connector type has been
available for some time as a module combining the input/output
connector with fuseholders, switches and indicators. These Polysnap modules
offer greatly reduced ‘real estate’ and reduced
assembly time as only a single panel cut-out is needed and
only one component is assembled into this cut-out. The latest Polysnap is
now available with miniature circuit breakers. The MCB provides
both circuit protection, switching and, if required, neon
illumination. The other benefit of this method of circuit
protection is an easy re-set eliminating the need to call
out service engineers to change fuses. The thermally operated
circuit breakers have UL & CSA
approvals offering reliable circuit protection that is commercially
attractive. Two major connector options are available; Standard
C14 type inlets, rated at 10A, 250V, or the higher power
C20 type inlets, rated at 16A, 250V, both are offered with
single pole circuit breakers, red illumination using 250V
neons or non-illuminated. The circuit breakers are available
with the following current ratings: 5A, 10A & 16A for
the C20 connector versions and 5A, 8A & 10A for the C14
versions.
C20
Mains Inlet Module
 |
• For
use with equipment requiring higher currents than currently
available
• from
standard IEC 60320 C13/14 types
• Illuminated or non illuminated switch with or without circuit breaker
Applications include
• Industrial equipment • Office equipment • Medical equipment |
Technical
Data
| Voltage
Rating |
250V
(UL, CSA, VDE) |
| Current
Rating |
16A
(VDE) 20A (UL, CSA) |
| High
in-rush switch |
150A
to IEC65 |
| Tag
size |
6.3mm
on all component |
| Order
Code |
Bulgin
P/N |
Type |
1+ |
5+ |
100+ |
| |
IEC
with Switch |
|
| 7325037 |
BZV49/Z0000098 |
Non
illuminated |
4.44 |
3.71 |
3.19 |
| 7325045 |
BZV49/Z0000/71 |
Red
Neon |
4.85 |
4.05 |
3.48 |
| |
IEC
with Circuit Breaker |
|
| 7325053 |
BZV49/Z0000/C1Q |
Non-illuminated.
Trip Current 5A |
8.37 |
6.98 |
6.01 |
| 7325061 |
BZV49/Z0000/C1U |
Non-Illuminated
Trip Current 10A |
8.37 |
6.98 |
6.01 |
| 7325070 |
BZV49/Z0000/C1Y |
Non-Illuminated
Trip Current 16A |
8.37 |
6.98 |
6.01 |
| 7325088 |
BZV49/Z0000/C4Q |
Red
Neon . Trip Current 5A |
8.93 |
7.45 |
6.41 |
| 7325096 |
BZV49/Z0000/C4U |
Red
Neon . Trip Current 10A |
8.93 |
7.45 |
6.41 |
| 7325100 |
BZV49/Z0000/C4Y |
Red
Neon . Trip Current 16A |
8.93 |
7.45 |
6.41 |
C14
Mains Inlet Module
 |
• Suitable
for equipment requiring re-settable circuit protection
on standard
• mains
connections
Applications include
• Industrial equipment • Office equipment • Medical equipment |
Technical
Data
| Voltage
Rating |
250V
(UL, CSA, VDE) |
| Current
Rating |
10A
(VDE) 15A (UL, CSA) |
| High
in-rush switch |
150A
to IEC65 |
| Tag
size |
6.3mm
on all component |
Farnell
order Code and Manufacturers List Numbers.
| Order
Code |
Bulgin
P/N |
IEC
with Circuit Breaker |
1+ |
5+ |
100+ |
| 7325118 |
BZV03/Z0000/C1Q |
Non-Illuminated
Trip Current 5A |
7.32 |
6.11 |
5.25 |
| 7325126 |
BZV03/Z0000/C1T |
Non-Illuminated
Trip Current 8A |
7.32 |
6.11 |
5.25 |
| 7325134 |
BZV03/Z0000/C1U |
Non-Illuminated
.Trip Current 10A |
7.32 |
6.11 |
5.25 |
| 7325142 |
BZV03/Z0000/C4Q |
Red
Neon. Trip Current 5A |
7.94 |
6.62 |
5.70 |
| 7325150 |
BZV03/Z0000/C4T |
Red
Neon Trip Current 8A |
7.94 |
6.62 |
5.70 |
| 7325169 |
BZV03/Z0000/C4U |
Red
Neon Trip Current 10A |
7.94 |
6.62 |
5.70 |
Ethernet
Buccaneer
Sealed In–Line LAN / Ethernet Cable Joiner
Ethernet
Buccaneer for Industrial Networks
Ethernet Buccaneer is an environmentally sealed circular
connector family offering protection to IP68. It is a fully
shielded (F-STP) system performing to Cat5e levels using
the proven RJ45 connector as the basis of the connection
technology. This is combined with the Buccaneer characteristics
to offer a secure, reliable and practical solution in the
Industrial environment. |
|
The RJ45 connector, together with twisted pair cabling,
has become standard for local area networks in office and
business environments. This well-known combination has become
the standard for Ethernet networks, but it's this very familiarity
that can lead to problems when used in Industrial situations.
The standard RJ45 connector and its associated cabling are
often too delicate and do not provide enough protection against
the requirements imposed by harsher Industrial applications.
There are some major differences between the ‘benign’ office
environment and the rigours and requirements of the Industrial
environment, these can be categorised as:
- Dust
and Water
- EMC
- Oils/minerals
- Vibration
- Handling
Bulgin's Ethernet Buccaneer design addresses these differences
as follows;
Dust & Water – Dust
is not generally recognised as a problem, but in practice
contamination of the contact pins can have a serious corrosive
effect resulting in signal degradation or eventual failure.
Water or moisture is more obvious in terms of system performance
or integrity. This not only makes a sealed connector system
essential, but also has implications for the cable jacket
and it's resistance to long term immersion. BS EN60529 defines
the degree of environmental protection, and sets out the
IP rating system. Ethernet Buccaneer offers IP68 protection;
dustproof and waterproof, with a submersion test at a depth
in excess of 2 metres - more than enough for most Industrial
or external applications.
EMC – noise (R.F.I.) from external sources can effect
data transmission, especially in electrically noisy environments
such as the shop floor. A well shielded, braided cable will
reduce interference susceptibility as will complete screening
of the connector system. Ethernet Buccaneer utilises cable
with an overall foil screen plus an overall braid (S-FTP)
with shielded RJ45 connectors to maintain continuity of the
screen through the entire Patchcord and through into the
equipment with a fully shielded coupler. These measures will
maintain the Faraday cage effect along the signal path, reducing
EMI to a minimum.
Oils and Minerals – it is important to ensure that
both the cable and the connector are resistant to any oils,
etc likely to be found in the system's operating environment.
The Ethernet Buccaneer housing is moulded in a tough UL94V-0
rated Polyester to give a high immunity to most commonly
found oils, minerals and chemicals. Polyethylene (PE) jacket
cable provides good levels of resistance to water, oils and
chemicals and will not crack with long exposure to water
or UV.
Vibration – the Ethernet Buccaneer uses a screw coupling
to ensure that connectors are mated properly and securely.
The cable retention at the rear of the re-wireable connector
must provide sufficient security to hold the cable securely,
to resist pulling, but without too great a pressure as this
could compress the cable, potentially degrading the data
transmission and so system performance. This can often be
overlooked when using re-wireable connectors and over-tightening
the clamping mechanism to achieve a cable seal. The Ethernet
Buccaneer has a cable gland and gland nut that are tuned
and tested to work specifically with the designated cable
constructions.
 |
PX0834 |
 |
PX0833 |
 |
PX0832 |
 |
PX0835 |
 |
PX0777 |
Handling – this is probably one of the most overlooked
areas. Both the cable and the connector can suffer from the
rigours of mis-use in an Industrial situation. Ethernet Buccaneer
considers this aspect critical for longer operational life.
The cable is an obvious consideration and UV/ozone resistance,
abrasion resistance and prolonged exposure to water can only
be resolved with quality cable constructions. For this reason
Ethernet Buccaneer uses PE jacket cables to offer performance
balanced with commercial considerations.
Perhaps the most important factor under this heading is
that of mechanical handling; the rough treatment that the
delicate RJ45 could see during mating or ‘blind mating’ or
even by being dropped on concrete floors. Ethernet Buccaneer
has a shroud that protects the RJ45 from this potential damage
and provides positive alignment during mating, guiding the
two connectors together and eliminating ‘mis-mating’.
The Ethernet Buccaneer range includes:
- Field re-wireable connector, PX0834/B, complete with
shielded RJ45
- Panel mounted connector, PX0833, housing
a Cat5e shielded coupler, this provides a sealed Buccaneer
connection to the front of the panel and a standard RJ45
to the rear. Single hole fixing makes it easy to fit
and the panel cut-out is compatible with all existing Standard
Buccaneer chassis
connectors. This is supplied complete with panel gasket.
- Standard length patch-cords in 2, 3 and 5 metre lengths.
These are available in double ended, Ethernet Buccaneer
to Ethernet Buccaneer (PX0832), or single ended, Ethernet
Buccaneer to standard RJ45 (PX0831).
- A new sealing cap
PX0835 is required for the flex connectors to maintain
IP rating when not mated. The chassis connector uses
the standard PX0733 sealing cap.
- This Ethernet Buccaneer
range has been complemented by the addition of a unique
in-line connection. Designed as a low cost cable joiner
using industry standard couplers protected by the proven Buccaneer cable
joiner housing (PX0777). Available supplied complete with
shielded (STP) and un-shielded (UTP) couplers or a high performance
shielded (STP) coupler rated to CAT5e levels. The in-line
LAN coupler is designed for use with all standard RJ45 connectors.
Technical
Data
| Rating |
1.5A,
30V ac., 42V d.c. |
| Housing
Material |
Glass
filled Polyamide UL94V-0 |
| Operating
Temperature |
-20
C to + 70 C |
| No
of Conductors |
8 |
Order
Codes and Manufacturers List Numbers
Mftrs List No |
Order |
Description |
1+ |
25+ |
50+ |
Buccaneer
PX0834/B
|
4285864 |
Re-wireable
Connector |
10.19 |
9.75 |
7.74 |
PX0833 |
4285852 |
Panel Mounting Connector |
20.8 |
19.26 |
15.39 |
PX0835 |
4285876 |
Sealing cap for flex connectors |
0.99 |
0.94 |
0.75 |
PX0831/2M00 |
4285888 |
Single ended patchcord
2m |
18.41 |
17.04 |
13.62 |
PX0831/3M00 |
4285890 |
Single ended patchcord
3m |
19.55 |
18.1 |
14.47 |
PX0831/5M00 |
4285906 |
Single ended patchcord
5m |
20.8 |
19.26 |
15.39 |
PX0832/2M00 |
4285918 |
Double ended patchcord
2m |
18.72 |
17.33 |
13.85 |
PX0832/3M00 |
4285920 |
Double ended patchcord
3m |
19.76 |
18.3 |
14.62 |
PX0832/5M00 |
4285931 |
Double ended patchcord
5m |
20.8 |
19.26 |
15.39 |
PX0733 |
314390 |
Sealing cap for panel
connector |
0.59 |
0.56 |
0.51 |
In-line
coupler |
|
|
|
|
|
PX0777/UTP |
7325177 |
In-line coupler - unshielded |
6.2 |
5.52 |
4.59 |
PX0777/STP |
7325185 |
In-line coupler - shielded |
8.45 |
7.53 |
6.26 |
PX0777/CAT5ESTP |
7325193 |
In-line coupler - shielded
CAT5e |
10.88 |
9.69 |
8.06 |
|